cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX support ST7796 or not ?

non
Associate III

i have stm32h750vbt6 and i want applied with TFT screen http://www.lcdwiki.com/4.0inch_SPI_Module_ST7796

in test demo is work then i don't know can use with TouchGFX or not

1 ACCEPTED SOLUTION

Accepted Solutions
Romain DIELEMAN
ST Employee

Hi,

TouchGFX works with any Parallel RGB (LTDC), MIPI DSI, FMC or SPI displays. So yes your display will work.

/Romain

View solution in original post

4 REPLIES 4
Romain DIELEMAN
ST Employee

Hi,

TouchGFX works with any Parallel RGB (LTDC), MIPI DSI, FMC or SPI displays. So yes your display will work.

/Romain

Do you have a sample link? Because I only have the library I found from the website I attached. The examples I found only ST7735 ILI8488 did not find ST7736.

ili9488 and ili7796 are very similar, the only difference between the two is the initial code,You can refer to the appropriate routines in www.lcdwiki.com website