Skip to main content
non
Associate III
May 17, 2023
Solved

TouchGFX support ST7796 or not ?

  • May 17, 2023
  • 1 reply
  • 4417 views

i have stm32h750vbt6 and i want applied with TFT screen http://www.lcdwiki.com/4.0inch_SPI_Module_ST7796

in test demo is work then i don't know can use with TouchGFX or not

This topic has been closed for replies.
Best answer by Romain DIELEMAN

Hi,

TouchGFX works with any Parallel RGB (LTDC), MIPI DSI, FMC or SPI displays. So yes your display will work.

/Romain

1 reply

Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
May 18, 2023

Hi,

TouchGFX works with any Parallel RGB (LTDC), MIPI DSI, FMC or SPI displays. So yes your display will work.

/Romain

non
nonAuthor
Associate III
May 18, 2023

Do you have a sample link? Because I only have the library I found from the website I attached. The examples I found only ST7735 ILI8488 did not find ST7736.

cchar.2
Associate
May 23, 2023

ili9488 and ili7796 are very similar, the only difference between the two is the initial code,You can refer to the appropriate routines in www.lcdwiki.com website