cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX project name in cubeIDE always the same: when will it be fixed?

Rodo
Senior

Hi all,

I'm new to touchGFX. I keep importing the very small projects I make (for STM32F746 Disco board) into the cubeIDE to test code. I read several posts that show how to fix the re-naming of the project so I can import the next test I try but they're cumbersome and you can't go back to the touchGFX project because of the filenames changes. I just saw that there is a new minor version change in touchGFX (from 4.21.4 to 4.22.0) but no fixes to this issue.

I'm wondering when will this import project name issue be fixed?

Thanks

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0