2020-06-08 10:33 AM
Hello,
On some of our old products, a small F103 was driving a TFT and also was getting the data to be printed (Strings,X-Y,Color etc) via UART from the [main] MCU.
We have changed the F103 with F746/F429i and running the TouchGFX but in order to keep the same logic and support the old firmware on main MCU (at least for now), we need to print Texts/Strings to display on the fly (same like we do on F103).
Is that possible with TouchGFX?
2020-06-11 1:48 AM
Hello,
Yes it is possible. You need to use wildcards with the TextArea widget.
Please refer to these links for more information:
https://support.touchgfx.com/docs/development/ui-development/ui-components/miscellaneous/text-area
/Alexandre
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.