Skip to main content
AS.19
Associate
January 4, 2023
Solved

TouchGFX on custom board

  • January 4, 2023
  • 6 replies
  • 2127 views

I am working on touchGFX on custom board where I am creating my project in CubeIDE.

I have integrated the touchGFX in .ioc file but when I try to compile the code in TouchGFX designer I get following error

  Post Generate Target

    touchgfx update_project

    Unable to locate D:/<project path>/.cproject

    Failed

  Failed

MORE:

Tried all suggestions from below link, but doesn't seem working.

https://community.st.com/s/question/0D53W00001SMGlCSAX/touchgfx-designer-error-unable-to-locate-cpathtofolder

Can someone suggest the solution for the same?

Or any demo project will be helpful.

This topic has been closed for replies.
Best answer by MM..1

Dual core projects is buggy from IDE, you need start opositte order as mentioned in other posts. (create from MX ...)

6 replies

MM..1
Super User
January 4, 2023

You complete lack info

versions, mcu , how you create project ...

AS.19
AS.19Author
Associate
January 4, 2023

Thank you for your reply!

I am using STM32H745BIT6.

CubeIDE 1.11.0

TouchGFX 4.21

CubeMX 6.7

Created project using CubeIDE, added TouchGFX component from device configuration tool(.ioc file)

Compiling the touchgfx project using TouchGFX Designer/Environment which I think is a standard way of generating files, where I get above error message.

Kept the question simple and generic, as a similar issue is mentioned in other community posts.

Please refer above link for similar issue.

MM..1
MM..1Best answer
Super User
January 5, 2023

Dual core projects is buggy from IDE, you need start opositte order as mentioned in other posts. (create from MX ...)

Osman SOYKURT
ST Technical Moderator
January 9, 2023

Hello AS.19,

I confirm that dual core project has a bit of complexity in the architecture.

As MM..1 said, you should create your project from STM32CubeMX and don't forget to uncheck the "Generate under Root" checkbox.

/Osman

ST Software Developer | TouchGFX
Richard Lowe
Senior II
February 27, 2024

Is there any work around or fix for this behavior?  Projects that are composed of linked files is a serious pain. I would like to generate the project under root so that I have 100% visibility to the files in my project.

 

AS.19
AS.19Author
Associate
January 9, 2023

Thanks @MM..1​  @Osman SOYKURT​ 

It's working now.