TouchGFX compile problems
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-02-24 7:18 AM
Hello, i am unable to compile a touchgfx project.
Try #1:
Starting from CubeMX, Version 6.10.0 i click on Generate Code. It ends with "The Code is successfully generated under:". When i click on Src/ApplicationTemplate.touchgfx.part, it opens TouchGFX Designer Version 4.23.1.
I start with a "Blank UI" and klick on Import.Then i define there a Box and a Button.
Then i click on "Generate Code" it fails with: Generate Code | Failed.
Unsupported toolchain: Makefile
Here the CubeMX is running on a linux box while TouchGFX Designer is running on a Windows 10 computer.
Try #2:
I import the .ioc file from CubeMX into STM32 CubeIDE version 1.14.0 with "Import an Existing STM32CubeMX Configuration File (.ioc). I choose target language C++. During import code is generated. The structure looks different compared to generated code in Try #1. When i click TouchGFX/ApplicationTemplate.touchgfx.part it opens TouchGFX Designer.
I start with a "Blank UI" and click on Import.Then i define there a Box and a Button.
Then i click on "Generate Code" it succeeds with "Generate Code | Done".
Back in CubeIDE i click on "Build Project" and it succeeds.
Does someone know how to generate a Makefile for CLI compilation?
Solved! Go to Solution.
- Labels:
-
STM32CubeMX
-
TouchGFX Designer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-04-10 1:21 AM
Hello @sk-st ,
That is great to hear!
So now you can do everything you want? Create a GUI and flash it, etc?
What are the adjustments that you had to do to the folders?
Regards,
Software engineer at ST (TouchGFX)

- « Previous
- Next »