2019-01-23 3:35 AM
I installed touch 4.10
select STM32429I-Disc1
after combining package:
1 At startup and when I pressed "Run Target" or "Generate Code" the program shows:
"Error during code generation".
2 When I pressed "Run Simulator":
"Unable to lounch simulator".
When forming a project from CubeMX, the same thing happens.
Does anyone know what's the matter?
2021-01-05 1:01 PM
Hi @Martin KJELDSEN ,
Im sorry. because im new for Touchgfx. so i dont know how i can do that. can you explain a little bit? :(
2021-01-05 11:46 PM
You have a TouchGFX environment installed along side the designer. You can execute make on our Makefiles to compile projects with gcc and arm-gcc. You should be able to find the program in your start menu,
/Martin
2021-01-07 6:08 AM
2021-01-12 11:44 AM
Hi again @Martin KJELDSEN ,
I understood how i can do environment and makefiles commands. but unfortunetly it was unsuccessfull.
I found some problems my project file. I added 2 files ; my home pc and my work pc screenshots. there is no some files such as build folders in my home pc. so i think touchgfx could not do compile and simulator. what do you think about that problem?
2021-01-12 11:44 AM
2021-01-12 12:56 PM
2021-01-12 3:19 PM
Hi. Jumping into the middle of this thread :)
Any reason as to why you are using the older version of the TouchGFX toolchain? The latest version is now 4.16.0. Been out of the loop for a bit and just updated my tools to the latest ST compiler and the TouchGFX 4.16.0. Ran a quick demo of the Pool Lights screen on our STM32F429 kit - ran fine.
Hope to use the latest suite of tools to build up some new code.
Can you upgrade your tools to the latest and just start with a simple example GUI?
So far from the very quick review today, the tools have come a long ways :) Very nice !!
Post your results after the upgrades..have the same kits here so perhaps we can help as we proceed with our development.
2021-01-12 10:00 PM
2021-01-12 11:53 PM
2021-01-13 12:07 AM
Hi @Mon2 ,
I made your suggests. I select and import "Pool Demo". gave below error ;
Run Simulator
Copy Framework
Copying TouchGFX framework version 4.16.0 to C:\TouchGFXProjects\MyApplication\Middlewares\ST\touchgfx
Done
Generate
Wrote config/gcc/app.mk
Wrote config/msvs/Application.props
Wrote generated/gui_generated/include/gui_generated/common/FrontendApplicationBase.hpp
Wrote generated/gui_generated/include/gui_generated/common/FrontendHeapBase.hpp
Wrote generated/gui_generated/include/gui_generated/common/SimConstants.hpp
Wrote generated/gui_generated/include/gui_generated/main_screen/MainViewBase.hpp
Wrote generated/gui_generated/include/gui_generated/pooltemp_screen/PoolTempViewBase.hpp
Wrote generated/gui_generated/src/common/FrontendApplicationBase.cpp
Wrote generated/gui_generated/src/main_screen/MainViewBase.cpp
Wrote generated/gui_generated/src/pooltemp_screen/PoolTempViewBase.cpp
Wrote generated/simulator/gcc/Makefile
Wrote generated/simulator/include/simulator/mainBase.hpp
Wrote generated/simulator/msvs/touchgfx.props
Wrote generated/simulator/msvs/touchgfx_prebuild.targets
Wrote generated/simulator/msvs/touchgfx_sdl2.props
Wrote generated/simulator/src/mainBase.cpp
Wrote generated/simulator/touchgfx.ico
Wrote generated/simulator/touchgfx.rc
Wrote generated/simulator/touchgfx.res
Wrote simulator/gcc/Makefile
Wrote simulator/main.cpp
Wrote simulator/msvs/Application.sln
Wrote simulator/msvs/Application.vcxproj
Wrote simulator/msvs/Application.vcxproj.filters
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Sistem belirtilen yolu bulamiyor.
Failed
Failed