Skip to main content
sandaruwan
Associate
December 13, 2023
Question

Touchgfx circular progress bar.

  • December 13, 2023
  • 4 replies
  • 3461 views

I'm using the stm32h750-dk development board and  TouchGFX 4.21.4 and STM32CubeIDE. I want to design a circular progress bar with a color gradient. I attached the required circular progress bar as an image. so I want to control the circular progress bar from the main.c using an external variable resistor. I'm Using the 'queue' to communicate between touch TouchGFX files and main.c file. Still, I can control the progress bar using a single color (without a color gradient). anyone can help me to implement a circular progress bar with a color gradient when progressing the bar.

image (25).png

 

this is the code that I use now.

 

void PageHomeView::updatePage(PageState *pageState)
{
      uint8_t index = pageState->buttonsState.index;
       circleProgress1.setValue(index);
}
 
I refer these links
This topic has been closed for replies.

4 replies

ST Employee
December 15, 2023

Hello @sandaruwan,

Unfortunately, there is no direct way to do it, and I don't have any solid ideas for doing it right now. But, I think if you use an image with gradient as your progress indicator, you might be able to get close to what you look for. 

I will update you if I found a solution.

Best regards

Mohammad MORADIST Software Developer | TouchGFX
Associate III
August 2, 2024

I came here for a different reason and this was the exact same thing I though about when I saw the post.

sandaruwan
Associate
December 15, 2023

Thanks your response @Mohammad MORADI ESFAHANIASL . please let me know if you find any solution. not possible to use images with gradient because the gradient area is dynamically changing with the progress value. 

ST Employee
December 18, 2023

I see. I will surely update you
Good luck

Mohammad MORADIST Software Developer | TouchGFX