2024-07-25 4:01 AM - last edited on 2024-08-05 3:19 AM by Andrew Neil
2024-08-02 5:46 AM - edited 2024-08-02 5:49 AM
Hello @Shivani ,
Both of the MCUs that you mentioned are excellent choices for graphics since they both support the Neo-Chrome accelerator. TouchGFX already have board setups ready for STM32H7S78 DK and STM32U5G9J DK2 to start developing your GUI as fast as possible, and Neo-Chrome is fully supported.
Board Setup for STM32H7S78 DK
Board Setup for STM32U5G9J DK2
Here you can read about the new features of TouchGFX 4.24.0
And about the frame rotation, I'm not sure exactly what you would like to achieve, but TouchGFX only supports display in portrait and landscape (so, 90-degree rotation).
Unfortunately, I don't have enough information about the state of QT, therefore I can't help with that.
Best regards,