2023-05-04 12:05 AM
Hello,
I use ToucheGFXDesigner 4.21.3 for the first time.
I have no problem to design the application for the 2 buttoms Run Simulator and Run Target are not Highlitghted. When, I point these buttoms, it's written : Can't run Simulator and Can't run target. Samething in the menu Code
I probably miss something but what?
If somebody coul help ?
Best Regards
Robert
2023-05-06 10:29 AM
Hello. Good that you get forward :thumbs_up: I dont have ideas about deleting 4 files, maybe somebody else can help you, maybe somebody have use TGFX with Win 11.
2023-05-06 11:58 PM
Hello JTP,
For your information, the issue is solved.
After your idea to cancel the 4 blocking files, I was able tu run completly TouchGFX with any project.
Then, I try to run in Stm32CubeIde. When, I open the .ioc file, the system ask for a major update (1GB). Everything was fine, I started to debug. The system ask for a firmare update of the Stm32LINK probe ( included in the board).
After that, I run the project from Stm32CubeIde. Everything was fine and the demo is perfect on the board.
Then, I redo the TouchGFX simulation. The 4 blocking files are no more blocking.
My understanding now is the firmware update of the Stm32LINK probe is the key point.
Thanks again for your support
Best regards