2021-07-24 12:48 AM
Hi,
when TouchGFX 4.17.0 is opened I'm getting an error stating no internet connectivity even though my laptop is connected to internet . also in the selection of boards I'm not getting any board option .
thanks and regards
sinduja
Solved! Go to Solution.
2021-09-27 03:57 AM
Hi,
any update concerning the tpa-file for STM32G071-NUCLEO-DEMO?
When will the problem with proxy login be fixed in TouchGFX designer?
Thanks.
2021-09-27 06:56 AM
2021-10-06 04:14 AM
Hi,
unfortunately, your file STM32G071-NUCLEO-DEMO-3.0.1.tpa is not recognized by TouchGFX 4.170.0 Designer.
Can you please upload a suitable version for 4.17.0?
Thanks.
2021-10-07 03:30 AM
Hi,
The file does work on my side this is strange. Just to be sure are you looking in the right place ? The nucleo demo you asked is found under the Board Specific Demo tab in the Demos section.
/Romain
2021-10-07 03:33 AM
2021-10-07 05:06 AM
Hello,
I wanted to create a new application (starting from a blank screen) for X-NUCLEO-GFX01M1 (STM32G071-Nucleo):
Create New => Show All => STM32G071-Nucleo did not appear with your originally uploaded STM32G071-NUCLEO-DEMO-3.0.1.tpa.
Then I realized that tpa is just a zip.file and that it contains a json file. In this json file, I changed
"Type": "TGAPP"
to
"Type": "TGAT"
and zipped it to a tpa file again.
After that the board appeared in "Create New" dialog.
So now it works for me.
Thanks.
2021-10-07 05:35 AM
Board specific demos do not appear when you go in the "Create New" section, it will only show TBS. I guess you were looking for the STM32G0 Nucleo tbs instead then, good to hear you were able to adapt it and that it works :thumbs_up:
/Romain
2021-10-07 05:44 AM
OK, and what is the difference between the "STM32G0 Nucleo tbs" and the STM32G071-NUCLEO-DEMO-3.0.1.tpa?
Can you please also upload "STM32G0 Nucleo tbs"?
Thanks.
2021-10-19 06:51 AM
> The issue should be fixed with the release of TouchGFX 4.18
Hi,
when will TouchGFX 4.18 be released?
Thanks.
2021-10-21 02:36 AM
Today normally ;)
/Romain