2020-01-27 09:50 PM
Hello I am trying to use Touch GFX. In CubeMX I installed the related software pack:
When I open the additional software part there is no option I can enable Touch GFX, it is simply empty:
How can I enable it from CubeMX? Thank you beforehand.
Solved! Go to Solution.
2020-01-28 02:36 AM
If you're using a dual core like H747, then no additional software is available from CubeMX - Which MCU is this?
/Martin
2020-01-28 02:36 AM
If you're using a dual core like H747, then no additional software is available from CubeMX - Which MCU is this?
/Martin
2020-01-28 02:46 AM
Yes it is dual core: STM32H747XIHx.
2020-01-28 02:49 AM
Sorry, CubeMX is blocking any additional software from being used in this case :( I'm not sure when that'll change or the reason for doing so outside of the dual cores being really complex.
2020-01-28 02:51 AM
Is there any way can I follow in order to use Touch GFX in dual core device without using CubeMX?
2020-01-28 02:53 AM
Not at the moment, but we have H747 disco and eval application templates ready through the touchgfx designer if you want to try that, but you cannot use the TouchGFX Generator with it unfortunately
I'll try to update on the status from CubeMX on allowing additional software for dual cores.
2020-01-28 03:04 AM
Thank you Martin :) appreciate it.
2020-04-17 01:15 PM
@Martin KJELDSEN Is there any update on it? It has been 3 months now, I know we are all struggling right now and such but are there any hopes it would finally work for H747 disco?
BR Pawel
2020-04-20 12:09 AM
I could ask around. You cannot enable additional software for H747 dual core in CubeMX - That's not in my power to change.
2020-04-20 12:24 AM
Q4'2020 - Straight from the CubeMX team.