2020-07-06 4:16 AM
Hi
In the TouchGFX Designer is it possible to set the text configuration to "Remap texts" and "A4" and it works well when I'm generating the code.
But when I build within VisualStudio these settings will not applied, even they are added within the "application.config" file.
Has anyone an idea where the problem can be?
/Marco
2020-07-06 6:43 AM
I just to verify, but i think this is a bug that we just fixed for 4.14.0
/Martin
2020-07-06 6:46 AM
Sounds good. When will 4.14. be available?
/Marco
2020-07-06 11:41 PM
Week 31 :)