2024-07-08 12:04 AM
How to change the alignment of textarea from the default style set in touchgfx designer?
In touchgfx designer(Version:4.21.3) I have set to Left alignment. I use this textarea for multiple purposes, for few I need to set to Left alignment and for few I need to set to Right alignment. I tried using ' textArea.setTextAlignment(TEXT_ALIGNMENT_RIGHT);' but it says set alignment is not a member.
Solved! Go to Solution.
2024-07-08 6:42 AM - edited 2024-07-08 11:38 AM
Hi @BhavyaSri
I use TextAreaWithOneWildcard
// T_ALIGN_LEFT, T_ALIGN_CENTER, T_ALIGN_RIGHT Ids text is "<>" with different alignment
// T_TEXT_MULTIALIGN holds the text to dispaly and alignment does not matter
TextAreaWithOneWildcard::setTypedText ( touchgfx::TypedText ( T_ALIGN_CENTER ) );
TextAreaWithOneWildcard::setWildcard ( touchgfx::TypedText ( T_TEXT_MULTIALIGN ).getText () );
TextAreaWithOneWildcard::invalidate ();
Example:
2024-07-08 6:19 AM
Hello @BhavyaSri ,
I have not seen a method called "setTextAlignment' in the textArea API.
You could try the method resizeToCurrentTextWithAlignment().
I think you should set the alignment directly from Designer instead of code.
If this comment solves your problem, I invite you to select it as "best answer".
Regards,
2024-07-08 6:27 AM
Thanks for your reply!
I cannot use from designer as I use Same textarea for multiple applications. Some of them need it to be right justified and some of them need it to be Left Justified. I have default set it as Left justified in designer, however for some cases I want to change that to Right justified via code.
Regards,
Bhavya
2024-07-08 6:42 AM - edited 2024-07-08 11:38 AM
Hi @BhavyaSri
I use TextAreaWithOneWildcard
// T_ALIGN_LEFT, T_ALIGN_CENTER, T_ALIGN_RIGHT Ids text is "<>" with different alignment
// T_TEXT_MULTIALIGN holds the text to dispaly and alignment does not matter
TextAreaWithOneWildcard::setTypedText ( touchgfx::TypedText ( T_ALIGN_CENTER ) );
TextAreaWithOneWildcard::setWildcard ( touchgfx::TypedText ( T_TEXT_MULTIALIGN ).getText () );
TextAreaWithOneWildcard::invalidate ();
Example:
2024-07-08 7:56 AM - edited 2024-07-08 8:49 AM
Attached is Gfx project with extension .pdf - rename it to .zip. Forum does not allow me to attach file with .zip. Strange as I see .zip files shared here.
2024-07-08 7:58 AM
2024-07-08 8:04 AM
Hi @ferro ,
I'm not able to see .pdf also. I'm able to see only image.
Also, just to add more details to my query:
1. I used textArea1 text field and enabled it as WildCard Buffer is designer.
2. I use 'Unicode::strncpy(textArea1Buffer,textfieldval, TEXTAREA1_SIZE);' in code and this 'textfieldval' will be changed based on microcontroller output.
Please let me know if additional details are required.
2024-07-08 8:37 AM
Hello @ferro ,
The ".zip" extension is not supported. Most people use the ".7z" extension to share their files.
Regards,
2024-07-08 8:38 AM
One simple fix would be to have 2 textAreas. one aligned left and one aligned right and just show the one you need at the time.
But Ferro's solution might be better and cleaner.
Regards,
2024-07-08 8:42 AM
Thanks @GaetanGodart , I see. I saw shared .zip on 'share your widget' thread but that was 2022, it's changed since then.