cancel
Showing results for 
Search instead for 
Did you mean: 

Text Area alignment change

BhavyaSri
Associate III

How to change the alignment of textarea from the default style set in touchgfx designer?

 

In touchgfx designer(Version:4.21.3) I have set to Left alignment. I use this textarea for multiple purposes, for few I need to set to Left alignment and for few I need to set to Right alignment. I tried using ' textArea.setTextAlignment(TEXT_ALIGNMENT_RIGHT);'  but it says set alignment is not a member.

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @BhavyaSri 

I use TextAreaWithOneWildcard

 

 

// T_ALIGN_LEFT, T_ALIGN_CENTER, T_ALIGN_RIGHT Ids text is "<>" with different alignment // T_TEXT_MULTIALIGN holds the text to dispaly and alignment does not matter TextAreaWithOneWildcard::setTypedText ( touchgfx::TypedText ( T_ALIGN_CENTER ) ); TextAreaWithOneWildcard::setWildcard ( touchgfx::TypedText ( T_TEXT_MULTIALIGN ).getText () ); TextAreaWithOneWildcard::invalidate ();

 

 

Example:

ferro_0-1720463890528.png

 

View solution in original post

14 REPLIES 14
GaetanGodart
ST Employee

Hello @BhavyaSri ,

 

I have not seen a method called "setTextAlignment' in the textArea API. 

You could try the method resizeToCurrentTextWithAlignment().
I think you should set the alignment directly from Designer instead of code.

 

If this comment solves your problem, I invite you to select it as "best answer".

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

Thanks for your reply!

 

I cannot use from designer as I use Same textarea for multiple applications. Some of them need it to be right justified and some of them need it to be Left Justified. I have default set it as Left justified in designer, however for some cases I want to change that to Right justified via code.

 

Regards,

Bhavya

Hi @BhavyaSri 

I use TextAreaWithOneWildcard

 

 

// T_ALIGN_LEFT, T_ALIGN_CENTER, T_ALIGN_RIGHT Ids text is "<>" with different alignment // T_TEXT_MULTIALIGN holds the text to dispaly and alignment does not matter TextAreaWithOneWildcard::setTypedText ( touchgfx::TypedText ( T_ALIGN_CENTER ) ); TextAreaWithOneWildcard::setWildcard ( touchgfx::TypedText ( T_TEXT_MULTIALIGN ).getText () ); TextAreaWithOneWildcard::invalidate ();

 

 

Example:

ferro_0-1720463890528.png

 

ferro
Lead

@BhavyaSri 

Attached is Gfx project with extension .pdf - rename it to .zip. Forum does not allow me to attach file with .zip. Strange as I see .zip files shared here.

ferro_0-1720450432559.png

 

Hi @GaetanGodart

Do you know why my .zip file attachments are refused by forum ? Thanks.

 

ferro_1-1720450675466.png

 

BhavyaSri
Associate III

Hi @ferro ,

I'm not able to see .pdf also. I'm able to see only image.

Also, just to add more details to my query:

1. I used textArea1 text field and enabled it as WildCard Buffer is designer.

2. I use 'Unicode::strncpy(textArea1Buffer,textfieldval, TEXTAREA1_SIZE);' in code and this 'textfieldval' will be changed based on microcontroller output.

Please let me know if additional details are required.

Hello @ferro ,

 

The ".zip" extension is not supported. Most people use the ".7z" extension to share their files.

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

One simple fix would be to have 2 textAreas. one aligned left and one aligned right and just show the one you need at the time.

But Ferro's solution might be better and cleaner.

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

Thanks @GaetanGodart , I see. I saw shared .zip on 'share your widget' thread but that was 2022, it's changed since then.

ferro_0-1720453303510.png