2024-12-20 5:33 AM - edited 2024-12-20 5:35 AM
Attached SVG image with vertical gradient renders correctly in TouchGFX Designer 4.24.1, but not in the simulator.
In simulator the gradient is horizontal in landscape mode and vertical in portrait mode.
Edit. SVG attachments are banned, but renaming it to TXT is banned too so my attachment wasn't attached.
"The attachment's gradient.svg.txt content type (text/plain) does not match its file extension and has been removed."
So I've attached it as source code:
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<!DOCTYPE svg PUBLIC "-//W3C//DTD SVG 1.1//EN" "http://www.w3.org/Graphics/SVG/1.1/DTD/svg11.dtd">
<svg width="400" height="100" xmlns="http://www.w3.org/2000/svg" xmlns:xlink="http://www.w3.org/1999/xlink">
<defs>
<linearGradient id="grad1" x1="0%" y1="0%" x2="0%" y2="100%">
<stop offset="0%" stop-color="yellow" />
<stop offset="50%" stop-color="green" />
<stop offset="100%" stop-color="red" />
</linearGradient>
</defs>
<rect width="200" height="100" x="10" y="10" fill="url(#grad1)"/>
</svg>
Solved! Go to Solution.
2025-03-05 2:43 AM
Hello @unsigned_char_array ,
TouchGFX 4.25.0 fixes the issue.
Regards,
2024-12-27 4:38 AM
Hello @unsigned_char_array ,
We are currently working on a similar issue with SVG which might be related to your or be the same issue.
I will keep you updated once we fix it.
Regards,
2025-01-21 3:07 AM
Hello @unsigned_char_array ,
Just to keep you updated, we have spotted some bugs with SVG and are fixing them.
Your issue should be part of them, I don't know exactly when it will be fixed but it will happen! :)
Regards,
2025-03-05 2:43 AM
Hello @unsigned_char_array ,
TouchGFX 4.25.0 fixes the issue.
Regards,
2025-03-05 3:41 AM
@GaetanGodart wrote:TouchGFX 4.25.0 fixes the issue.
Confirmed. Tested with a devboard and simulator. Both landscape and portrait render properly.