2022-04-07 4:07 PM
MCU: STM32L4R9ZIJ6
PSRAM: APS1604M-3SQR-SN
Display: 800x480, RGB888, 24-bit
Hi, I'd like to use the mentioned PSRAM to store the TouchGFX framebuffer using OCTOSPI in QuadSPI mode.
I have tried setting the Frame Buffer Start Address to
OCTOSPI1_BASE (0x90000000), but that does not seem to work. I only get junk data.
I have read the TouchGFX docs, LTDC datasheets, and OSPI datasheets very thoroughly, and still cannot figure it out.
Additional Q's:
Note: I am using a custom board/application. Please assume the hardware is correct for the sake of discussion.
Any help would be appreciated. If any further clarification is needed please ask. I will include an image of the LCD display image as it stands.
2022-04-07 6:44 PM
>>How does the MCU "know" an external PSRAM has been added?
You'd have BSP code initializing the clocks,pins and OSPI/OSPIM peripheral, bring-up/config memory, enable the memory-mapping.
If you don't initialize it on the MCU, it will Hard Fault
You can validate the memory works via data pattern testing.
2022-04-08 8:38 AM
Thank you for your response.
I've done the initializing through CubeMX with GPIO pins as such:
// octospi.c
/**OCTOSPI1 GPIO Configuration
PC11 ------> OCTOSPIM_P1_NCS
PF8 ------> OCTOSPIM_P1_IO0
PF6 ------> OCTOSPIM_P1_IO3
PF7 ------> OCTOSPIM_P1_IO2
PF10 ------> OCTOSPIM_P1_CLK
PF9 ------> OCTOSPIM_P1_IO1
*/Is there anything further I need to do?(Outside of the MX generated code)
I have tried the APS1604M-3SQR-SN example code on pg.57 of AN5050, but found nothing written to 0x90000000 upon inspection in the CubeIDE Memory Monitor.
2022-04-08 8:48 AM
I'm not familiar with your design/implementation.
If this is a custom design you'll likely have to do some validation
2022-04-08 8:56 AM
No worries. It is a custom design. I'm looking for software answers and assuming the hardware is correct. If all I need to do is setup OSPI in CubeMX then write to address 0x90000000 then that answers my question to a degree. Thank you.
2022-04-08 9:51 AM
It seems I'm having an issue between OSPI indirect mode and memory mapped mode. Memory mapped mode is read-only and likely works better for Flash memory, where Images and other TouchGFX things are stored. I am trying to use memory mapped mode to read the frame buffer, but since it is read only OSPI cannot "store" or write the frame buffer to the OSPI address 0x90000000.
I will try using indirect mode instead.
2022-04-08 10:17 AM
I'm not sure this L4+ device supports memory mapped read/write to RAM on the OctoSPI, read perhaps, write don't think so.
For DMA/LTDC operation it's going to need to be memory-mapped for those to read data.
The memory-mapped and command modes aren't exactly inter-operable.
The general expectation being that the display/frame buffer is within the internal SRAM, so that it's not constantly switching modes, and disturbing the painting of images onto the screen.
2022-07-04 2:23 PM
There are limitation with the STM32L4R... to use OPI & QSPI RAM.
This is solved with later STM32 (L5, U5, H7...)
Alex
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.