2026-02-04 6:12 AM
I'm currently using an STM32H7S78-DK, and I'm correctly able to run TouchGFX with FreeRTOS and everything. I also an error handler function that, in case of a crash of TouchGFX it writes directly to the framebuffer.
Now, I would like to do a similar thing but on the boot code, so basically before the classic jump if (BOOT_OK != BOOT_Application())
I have an external RAM mapped at the address 0x90000000 which works correctly in TouchGFX with .icf like
define symbol __region_EXTRAM_start__ = 0x90000000;
define symbol __region_EXTRAM_end__ = 0x91FFFFFF;
define region EXTRAM_region = mem:[from __region_EXTRAM_start__ to __region_EXTRAM_end__];
place in EXTRAM_region { first section TouchGFX_Framebuffer
, section Video_RGB_Buffer
, section Nemagfx_Stencil_Buffer };I wanted to use the same section of memory in the Boot, accessing the framebuffer directly, so I edited the .icf of the boot with
define symbol __region_EXTRAM_start__ = 0x90000000;
define symbol __region_EXTRAM_end__ = 0x91FFFFFF;
define region EXTRAM_region = mem:[from __region_EXTRAM_start__ to __region_EXTRAM_end__];
place in EXTRAM_region { first section Boot_Framebuffer };And in the main.c
#pragma location = "Boot_Framebuffer"
__no_init uint32_t frameBuf[(800 * 480 * 2 + 3) / 4 * 2];Using J-Link and IAR, during the debug, I'm seeing the frameBuf is correctly mapped from address 0x90000000 but, as soon as I try to access the memory address, for instance wiping the frameBuf with
memset((void*)frameBuf, 0, sizeof(frameBuf));The code goes into HardFault. I have set the correct address for the LTDC with
LTDC_Layer1->CFBAR = (uint32_t)frameBuf;
LTDC->SRCR = (uint32_t)LTDC_SRCR_IMR;and I'm correctly initializing the XSPI as they return HAL_OK
MX_XSPI1_Init(); // External flash
MX_XSPI2_Init(); // External PSRAMI've alos configured the MPU region for the EXT RAM with
static void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct = {0};
/* Disables the MPU */
HAL_MPU_Disable();
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER3;
MPU_InitStruct.BaseAddress = 0x90000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_32MB;
MPU_InitStruct.SubRegionDisable = 0x00;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL1;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}I suspect that the CPU does not have the address of the external RAM mapped in its internal registries; could it be? Is there a way to access this frame buffer and read/write it to/from the external RAM
Solved! Go to Solution.
2026-02-05 2:30 AM
The issue seemed to be that in the MX_EXTMEM_MANAGER_Init it wasn't defined
if (EXTMEM_MemoryMappedMode(EXTMEMORY_2, EXTMEM_ENABLE) != EXTMEM_OK)
{
Error_Handler();
}
2026-02-05 2:30 AM
The issue seemed to be that in the MX_EXTMEM_MANAGER_Init it wasn't defined
if (EXTMEM_MemoryMappedMode(EXTMEMORY_2, EXTMEM_ENABLE) != EXTMEM_OK)
{
Error_Handler();
}