2020-10-19 03:15 AM
I wanted to use the 8080 interface on the STM32H750 to drive the 5-inch LCD (800x480) and only use the MCU's internal SRAM.Is there a similar template for reference?Because all I can see are templates that use the LTDC(RGB888)+DMA2D+SDRAM interface.Thank you very much:D
2020-10-19 04:43 AM
I think you could probably fit one single B/W frame somehow but you will need lot's of ram for anything color.
2020-10-21 12:34 AM
I want to use 8080,RGB565, partial frame cache and DMA2D mode to drive THE LCD
2020-10-25 06:07 PM
😂