cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F469NI-Discovery kit unable to make the LTDC peripheral works.

DAngo.1
Associate

Hi I jist bought a STM32F469NI-Discovery board recently and I am unable to make the display work.

I started with the BSP libraries and examples and they worked fine. i even was able to modify a bit an example and start doing someting with it.

The problem is when I started to work with STM32CubeMX. Firsty I tried to set ereverything in the progrma and make it to generate te code. As it didn´t worked I copeid the code from the examples.

When I run a program that tries to set a yelllow rectangle with DMA2D this is what I get.

0693W000000Vof1QAC.jpg

I tried modifying the code but I got no progress.

I thinks it has to do with the SDRAM rather than the LTDC peripheral but I am not sure.

At this point I am stuck so any kep will be welcomed.

Thanks in advance

0 REPLIES 0