2019-02-20 09:30 PM
Hello.
I try to make application with USB FS (host msc) and emwin on board stm32h743i-eval.
When i connect USB, enumeration doesn't happen. Function USBH_Get_DevDesc always return USBH_BUSY, and usb stay in state ENUM_IDLE.
But if i comment function GUI_Init enumeration is ok and i can see some usb descriptors in my uart terminal. Something happening in GUI_Init, that prevents usb.
Another strange thing is that i also have USB (HS) Host camera device (UVC class), and it works fine with GUI_Init or without it.
So, this code works well:
SystemClock_Config();
__HAL_RCC_CRC_CLK_ENABLE();
//GUI_Init();
USBH_Init(&usb_storage_handle, usb_storage_process, USB_STORAGE_ID);
USBH_RegisterClass(&usb_storage_handle, USBH_MSC_CLASS);
USBH_Start(&usb_storage_handle);
while (1) {
USBH_Process(&usb_storage_handle);
}
But when i change
//GUI_Init();
on
GUI_Init();
USB dont work.
Help me please. Thanks
2021-09-11 09:43 AM
Hi,
Have you been able to solve it?!
I have the same problem on STM32F469 + FreeTROS + STemWIN + USB device :(
Best regards Adam
2021-09-11 11:00 AM
Hi!
The USB host is very resource heavy on STM devices. I was able to run 1xUSB host + STemWin + FreeRTOS on STM32F746 board with more-or-less stable operation, but the same board simply does not draw out 2xUSB hosts + STemWin + FreeRTOS, choking with interrupt flood.
Maybe you could try some debugging? Could this be a problem with too heavy drawing task for Stemwin?
2021-09-24 07:53 AM
Hello everyone!
I found a solution to the problem.
The GUI_Init() function calls the functions: LCD_X_Config() from file: LCDConf.c.
I copied the above mentioned file from the demo.
In this file was changing clock settings. After blocking this part of the code everything started 🙂
See bellow:
/* LCD clock configuration */
/* PLLSAI_VCO Input = HSE_VALUE/PLL_M = 1 Mhz */
/* PLLSAI_VCO Output = PLLSAI_VCO Input * PLLSAIN = 384 Mhz */
/* PLLLCDCLK = PLLSAI_VCO Output/PLLSAIR = 384 MHz / 5 = 76.8 MHz */
/* LTDC clock frequency = PLLLCDCLK / LTDC_PLLSAI_DIVR_4 = 76.8 MHz / 2 = 38.4 MHz */
/*
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_LTDC;
PeriphClkInitStruct.PLLSAI.PLLSAIN = 384;
PeriphClkInitStruct.PLLSAI.PLLSAIR = 5;
PeriphClkInitStruct.PLLSAIDivR = RCC_PLLSAIDIVR_4;
HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct);
*/
Sometimes the simplest mistakes are the hardest to find! 😂
Best Regards to All