cancel
Showing results for 
Search instead for 
Did you mean: 

Settings problem in STemWin interface to LDTC for ILI9341

tamilselvansubramani1
Associate II
Posted on November 17, 2015 at 08:21

Hi,

I am working on

STM32F429 for LCD interface (LTDC).

LCD controller: ILI9341

Interface used: RGB

We are using STemWin li

brary for GUI interface.

We are able to work with GUIDRV_FLEXCOLOR_F66709 setting for 16 bit parallel interface.

But we could not map PortAPI parameters

(write16 bit data and read16bit) for GUIDRV_FlexColor_SetFunc() with RGB interface.

Can we use the GUIDRV_FLEXCOLOR_F66709

for RGB interface? If not, which should be setting for RGB interface?

Thanks in Advance.

By

Tamilselvan

#stemwin #ili9341 #ldtc
0 REPLIES 0