2025-02-07 2:12 PM
I am having trouble receiving data with my Riverdi Display rvt70hssfwca0. I am not sure if it is a software or a hardware problem since when I was testing the RS485 I shorted pin 2 (Signal A - Non inverting) and Pin 1 (Vin - 24V). When debugging this is what I observed.
I suspect either D4 or U2 damage might be blocking the signal somehow from going back to the MCU. But there is a possibility that I need to enable something in the MCU using software to disable high impedance, maybe? - Which I did, by setting PA15 low, right? I checked the DE and RE pins on U2 and the seem to set themselves on and off correctly at the same time when the display is outputting a signal. They are both on when transmitting, and off every other time.
I also looked into the rvt70hssfwca0 schematic but I could not find it. U2 is a (I believe) ST3485EBDR interface IC. I do not know what D4 is, yet.
Any help works!
Solved! Go to Solution.
2025-02-07 3:53 PM
Nevermind,
I decided to swap the ST3485E for a THVD1420DR I had available and it worked.
2025-02-07 3:53 PM
Nevermind,
I decided to swap the ST3485E for a THVD1420DR I had available and it worked.