QSPI Write Issue on STM32H745 with MT25QL512 in IAR
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-03 4:54 AM
Hello,
I am working on interfacing an external flash memory IC MT25QL512 with the STM32H745 microcontroller using QSPI in IAR Embedded Workbench.
The Problem:
When attempting to write data to the external flash using the HAL_QSPI_Transmit function, the operation fails at the following line:
status = QSPI_WaitFlagStateUntilTimeout(hqspi, QSPI_FLAG_TC, SET, tickstart, Timeout);
Details of My Setup:
- Microcontroller: STM32H745
- Flash Memory IC: MT25QL512
- Development Environment: IAR Embedded Workbench
- Has anyone encountered a similar issue with the QSPI_FLAG_TC not being set during a write operation?
- Are there specific configuration or timing considerations for the STM32H745 and MT25QL512 combination that I might be overlooking?
- Any debugging tips or suggestions would be greatly appreciated.
Thank you for your support!!
Solved! Go to Solution.
- Labels:
-
TouchGFX
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-03 5:22 AM - edited ‎2024-12-03 5:23 AM
Hard to say, you're pushing the content, so should have control of the speed of the transaction.
Are you placing a Debug View of the QSPI Peripheral Registers? Should probably avoid that due to secondary effects of the debugger, the status registers, and the data/FIFO registers.
Anything else trying to operate concurrently with the memory?
Able to get a logic analyzer on the pins?
Other code examples working? Clock/Peripheral enabled? ie non-zero content in registers and writable.
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
‎2024-12-03 5:22 AM - edited ‎2024-12-03 5:23 AM
Hard to say, you're pushing the content, so should have control of the speed of the transaction.
Are you placing a Debug View of the QSPI Peripheral Registers? Should probably avoid that due to secondary effects of the debugger, the status registers, and the data/FIFO registers.
Anything else trying to operate concurrently with the memory?
Able to get a logic analyzer on the pins?
Other code examples working? Clock/Peripheral enabled? ie non-zero content in registers and writable.
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
‎2024-12-03 9:10 PM
Attached IAR debug logs
0.001: File generated Wed Dec 4 10:36:52 2024
0.000: Pass 3 of 3
0.000: Starting fragment-style flashloader pass.
0.000: Device: C:\Users\harshal.gajjalwar\Desktop\External_IAR_LODER\FlashSTM32H745I-DISCO_QSPI_test.flash
0.001: Flash loader: C:\Users\harshal.gajjalwar\Desktop\External_IAR_LODER\FlashSTM32H7xx_QSPI_MICRON.out
0.154: FlashInitEntry is at 0x2400'25f4
0.154: FlashWriteEntry is at 0x2400'25fc
0.154: FlashEraseWriteEntry is at 0x2400'2604
0.154: FlashBreak is at 0x2400'00f8
0.154: FlashBufferStart is at 0x2400'4800
0.154: FlashBufferEnd is at 0x2404'0000
0.154: theFlashParams is at 0x2400'2644
0.154: FlashPreInitEntry not found
0.156: FlashChecksumEntry not found
0.156: FlashSignoffEntry not found
0.156: page size is 256 (0x100)
0.156: filler is 0xff
0.156: buffer size is 243712 (0x3'b800) 0.156:
0.156: Base of flash at 0x9000'0000
0.156: SimpleCode records (after offset):
0.156: Record 0: @ 0x9000'0000 [6824272 (0x68'2150) bytes] 0x9000'0000 - 0x9068'214f [0 0 0 0 ... ]
0.156: ->init : base @ 0x9000'0000, image size 0x68'2150
0.156: Store TargetParams to 0x2400'2644
0.157: Setting PC to 0x2400'25f4 (FlashInitEntry)
0.196: timing(init): 0.0000 (CPU) 0.0310 (elapsed)
0.196: Load TargetParams from 0x2400'2644
0.199: Transaction list:
0.199: Transaction 0: @ 0x9000'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9000'0000 (0x1'0000 bytes)
0.199: 1: 0x9001'0000 (0x1'0000 bytes)
0.199: 2: 0x9002'0000 (0x1'0000 bytes)
0.199: Transaction 1: @ 0x9003'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9003'0000 (0x1'0000 bytes)
0.199: 1: 0x9004'0000 (0x1'0000 bytes)
0.199: 2: 0x9005'0000 (0x1'0000 bytes)
0.199: Transaction 2: @ 0x9006'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9006'0000 (0x1'0000 bytes)
0.199: 1: 0x9007'0000 (0x1'0000 bytes)
0.199: 2: 0x9008'0000 (0x1'0000 bytes)
0.199: Transaction 3: @ 0x9009'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9009'0000 (0x1'0000 bytes)
0.199: 1: 0x900a'0000 (0x1'0000 bytes)
0.199: 2: 0x900b'0000 (0x1'0000 bytes)
0.199: Transaction 4: @ 0x900c'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x900c'0000 (0x1'0000 bytes)
0.199: 1: 0x900d'0000 (0x1'0000 bytes)
0.199: 2: 0x900e'0000 (0x1'0000 bytes)
0.199: Transaction 5: @ 0x900f'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x900f'0000 (0x1'0000 bytes)
0.199: 1: 0x9010'0000 (0x1'0000 bytes)
0.199: 2: 0x9011'0000 (0x1'0000 bytes)
0.199: Transaction 6: @ 0x9012'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9012'0000 (0x1'0000 bytes)
0.199: 1: 0x9013'0000 (0x1'0000 bytes)
0.199: 2: 0x9014'0000 (0x1'0000 bytes)
0.199: Transaction 7: @ 0x9015'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9015'0000 (0x1'0000 bytes)
0.199: 1: 0x9016'0000 (0x1'0000 bytes)
0.199: 2: 0x9017'0000 (0x1'0000 bytes)
0.199: Transaction 8: @ 0x9018'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9018'0000 (0x1'0000 bytes)
0.199: 1: 0x9019'0000 (0x1'0000 bytes)
0.199: 2: 0x901a'0000 (0x1'0000 bytes)
0.199: Transaction 9: @ 0x901b'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x901b'0000 (0x1'0000 bytes)
0.199: 1: 0x901c'0000 (0x1'0000 bytes)
0.199: 2: 0x901d'0000 (0x1'0000 bytes)
0.199: Transaction 10: @ 0x901e'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x901e'0000 (0x1'0000 bytes)
0.199: 1: 0x901f'0000 (0x1'0000 bytes)
0.199: 2: 0x9020'0000 (0x1'0000 bytes)
0.199: Transaction 11: @ 0x9021'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9021'0000 (0x1'0000 bytes)
0.199: 1: 0x9022'0000 (0x1'0000 bytes)
0.199: 2: 0x9023'0000 (0x1'0000 bytes)
0.199: Transaction 12: @ 0x9024'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9024'0000 (0x1'0000 bytes)
0.199: 1: 0x9025'0000 (0x1'0000 bytes)
0.199: 2: 0x9026'0000 (0x1'0000 bytes)
0.199: Transaction 13: @ 0x9027'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9027'0000 (0x1'0000 bytes)
0.199: 1: 0x9028'0000 (0x1'0000 bytes)
0.199: 2: 0x9029'0000 (0x1'0000 bytes)
0.199: Transaction 14: @ 0x902a'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x902a'0000 (0x1'0000 bytes)
0.199: 1: 0x902b'0000 (0x1'0000 bytes)
0.199: 2: 0x902c'0000 (0x1'0000 bytes)
0.199: Transaction 15: @ 0x902d'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x902d'0000 (0x1'0000 bytes)
0.199: 1: 0x902e'0000 (0x1'0000 bytes)
0.199: 2: 0x902f'0000 (0x1'0000 bytes)
0.199: Transaction 16: @ 0x9030'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9030'0000 (0x1'0000 bytes)
0.199: 1: 0x9031'0000 (0x1'0000 bytes)
0.199: 2: 0x9032'0000 (0x1'0000 bytes)
0.199: Transaction 17: @ 0x9033'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9033'0000 (0x1'0000 bytes)
0.199: 1: 0x9034'0000 (0x1'0000 bytes)
0.199: 2: 0x9035'0000 (0x1'0000 bytes)
0.199: Transaction 18: @ 0x9036'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9036'0000 (0x1'0000 bytes)
0.199: 1: 0x9037'0000 (0x1'0000 bytes)
0.199: 2: 0x9038'0000 (0x1'0000 bytes)
0.199: Transaction 19: @ 0x9039'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9039'0000 (0x1'0000 bytes)
0.199: 1: 0x903a'0000 (0x1'0000 bytes)
0.199: 2: 0x903b'0000 (0x1'0000 bytes)
0.199: Transaction 20: @ 0x903c'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x903c'0000 (0x1'0000 bytes)
0.199: 1: 0x903d'0000 (0x1'0000 bytes)
0.199: 2: 0x903e'0000 (0x1'0000 bytes)
0.199: Transaction 21: @ 0x903f'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x903f'0000 (0x1'0000 bytes)
0.199: 1: 0x9040'0000 (0x1'0000 bytes)
0.199: 2: 0x9041'0000 (0x1'0000 bytes)
0.199: Transaction 22: @ 0x9042'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9042'0000 (0x1'0000 bytes)
0.199: 1: 0x9043'0000 (0x1'0000 bytes)
0.199: 2: 0x9044'0000 (0x1'0000 bytes)
0.199: Transaction 23: @ 0x9045'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.199: Will erase 3 block(s):
0.199: 0: 0x9045'0000 (0x1'0000 bytes)
0.200: 1: 0x9046'0000 (0x1'0000 bytes)
0.200: 2: 0x9047'0000 (0x1'0000 bytes)
0.200: Transaction 24: @ 0x9048'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x9048'0000 (0x1'0000 bytes)
0.200: 1: 0x9049'0000 (0x1'0000 bytes)
0.200: 2: 0x904a'0000 (0x1'0000 bytes)
0.200: Transaction 25: @ 0x904b'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x904b'0000 (0x1'0000 bytes)
0.200: 1: 0x904c'0000 (0x1'0000 bytes)
0.200: 2: 0x904d'0000 (0x1'0000 bytes)
0.200: Transaction 26: @ 0x904e'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x904e'0000 (0x1'0000 bytes)
0.200: 1: 0x904f'0000 (0x1'0000 bytes)
0.200: 2: 0x9050'0000 (0x1'0000 bytes)
0.200: Transaction 27: @ 0x9051'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x9051'0000 (0x1'0000 bytes)
0.200: 1: 0x9052'0000 (0x1'0000 bytes)
0.200: 2: 0x9053'0000 (0x1'0000 bytes)
0.200: Transaction 28: @ 0x9054'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x9054'0000 (0x1'0000 bytes)
0.200: 1: 0x9055'0000 (0x1'0000 bytes)
0.200: 2: 0x9056'0000 (0x1'0000 bytes)
0.200: Transaction 29: @ 0x9057'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x9057'0000 (0x1'0000 bytes)
0.200: 1: 0x9058'0000 (0x1'0000 bytes)
0.200: 2: 0x9059'0000 (0x1'0000 bytes)
0.200: Transaction 30: @ 0x905a'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x905a'0000 (0x1'0000 bytes)
0.200: 1: 0x905b'0000 (0x1'0000 bytes)
0.200: 2: 0x905c'0000 (0x1'0000 bytes)
0.200: Transaction 31: @ 0x905d'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x905d'0000 (0x1'0000 bytes)
0.200: 1: 0x905e'0000 (0x1'0000 bytes)
0.200: 2: 0x905f'0000 (0x1'0000 bytes)
0.200: Transaction 32: @ 0x9060'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x9060'0000 (0x1'0000 bytes)
0.200: 1: 0x9061'0000 (0x1'0000 bytes)
0.200: 2: 0x9062'0000 (0x1'0000 bytes)
0.200: Transaction 33: @ 0x9063'0000 + 0x0 (0x3'0000=196608 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x9063'0000 (0x1'0000 bytes)
0.200: 1: 0x9064'0000 (0x1'0000 bytes)
0.200: 2: 0x9065'0000 (0x1'0000 bytes)
0.200: Transaction 34: @ 0x9066'0000 + 0x0 (0x2'2200=139776 bytes) 3 packet(s).
0.200: Will erase 3 block(s):
0.200: 0: 0x9066'0000 (0x1'0000 bytes)
0.200: 1: 0x9067'0000 (0x1'0000 bytes)
0.200: 2: 0x9068'0000 (0x1'0000 bytes)
0.222: ->multi_erase: 3 blocks (0x18 bytes in buffer) [0 0 0]
0.223: Store TargetParams to 0x2400'2644
0.224: Setting PC to 0x2400'2604 (FlashEraseWriteEntry)
0.273: timing(erase): 0.0000 (CPU) 0.0410 (elapsed)
0.274: Load TargetParams from 0x2400'2644
0.274: ->write : @ 0x9000'0000 (0x3'0000 bytes, offset 0x0 into block @ 0x9000'0000) [0 0 0]
0.274: Writing 0x3'0000 bytes to FlashBuffer @ 0x2400'4800
1.793: Store TargetParams to 0x2400'2644
1.795: Setting PC to 0x2400'25fc (FlashWriteEntry)
1.842: timing(write): 0.0000 (CPU) 0.0370 (elapsed)
1.842: Load TargetParams from 0x2400'2644
1.845: Func returned 4 (0 means Ok) 630_d_90000000
1.873: Flash loading pass finished
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-05 1:38 AM
Hello @Harsh_Gajjalwar ,
You have selected Tesla's answer as "best solution".
Where you able to fix your issue?
Regards,
Software engineer at ST (TouchGFX)