cancel
Showing results for 
Search instead for 
Did you mean: 

Data in RAM of stm32h7 gets messed up

ZY3
Associate

I wrote a code for stm32h745, masking the M4 core, and debugged it for two weeks without any problems per se, but yesterday, I realized that I could download the code, but in debug, I noticed that the data in RAM changes, and I didn't make any changes to that data, and I didn't have this problem before. My code hardly changes at all and I can rule out the out of address range issue. What is the reason for this. Is there any part of the chip that is damaged?

3 REPLIES 3
Uwe Bonnes
Chief

There are zillions of options, e.g.

unstable supplies, unconnected supply pins, missing decoupling capacitors, your program going amok, the debugger set up to use RTT, etc.

Pavel A.
Super User

DMA?

 

bramble
Senior

First thing to check is your stack allocation. A stack overflow call cause weirdly variable problems. 

Suspect the hardware as a last resort after you've checked everything else... it's almost certainly a software problem.

Somebody else mentioned DMA which you can check by disabling any peripherals that you may have configured to use it, and/or any DMA transfers in your application.

After that, you need to stare long and hard at anywhere you're writing to an array or raw pointer. You can also declare a dummy guard variable before and after any arrays, whether they're statically declared or malloc'd, write a magic value into them such as 0x12345678 then sprinkle in your code some checks to detect any unexpected change of those values.