cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with TouchGFX tutorial 3 - question marks instead of numbers

AWe.1
Associate II

Hello :)

I'm new with TouchGFX and I'm doing official TouchGFX tutorials.

I came up with the problem - code is properly generated and target/simulation can be run, but when I use buttons up/down then not number but question mark is displayed.

I'm using STM32F7508-DK.

0693W00000GZBZLQA5.jpgDoes anyone have any idea what is the problem?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
MM..1
Chief III

You need manage characters used in application fonts in designer typography lists. Not listed is replaced with ?

View solution in original post

2 REPLIES 2
MM..1
Chief III

You need manage characters used in application fonts in designer typography lists. Not listed is replaced with ?

AWe.1
Associate II

@MM..1​ It works! Thank you! :)