cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with "Run Target" on TouchGFX Designer: target/gcc/Makefile: No such file or directory

Alberto1
Associate III

I state that I have already seen this problem within the community, but I was unable to solve my problem.

I'm reading the TouchGFX Documentation to be able to develop an application: I followed the instructions in "Code Structure" with the simple example provided.

If I go to simulation, everything is ok.

If instead I try to execute "Run Target", I am returned:

compile

make -f target/gcc/Makefile -j8

make: target/gcc/Makefile: No such file or directory

make: *** No rule to make target 'target/gcc/Makefile'. Stop.

Failed

Checking in "Config" of the TouchGFX Designer, I noticed that the lines "Compile Target Command" and "Flash Target Command" are not compiled.

I entered "make -f target/gcc/Makefile -j8" and "make -f target/gcc/Makefile -j10 flash" respectively.

The result doesn't change.

I also noticed that while the gcc folder is present in the "simulator" folder, it is not present in the "target" folder.

How can I solve the problem? What does it depend on?

Thank you in advance.

Alberto

11 REPLIES 11

Hi!

Thanks for your reply and for the tips.

As you can understand I'm a newbie in TouchGFX.

Alberto

If you are working with an STM32H7B3dk board or a custom board with a similar display, I recommend to have a look at all the files in the TouchGFX/target folder of our example as this is where most of the user code is added to enable the display transfer and touch controller.

/Romain