2024-07-19 09:31 AM
Hello,
Let me describe the scenario
Version: 4.23.2
Succesfull Tests:
- Environment: Local Machine: Windows 11, touchgfx installed the same as using the dockerfile the command works
-Command Run:
-> powershell -Command 'C:\TouchGFX\4.23.2\designer\tgfx.exe generate -p C:\builds\TouchGFX'
Generates the files in the folder C:\builds\TouchGFX\generated
Issues:
- Environment: windows container based on image mcr.microsoft.com/windows:ltsc2019
- Installation method: Dockerfile, download the executable, place it on C:\install and running:
RUN msiexec /i "C:\install\TouchGFX-4.23.2.msi" /quiet /norestart
The Docker image builds ok and I have confirmed it has the .exe in the path C:\TouchGFX\4.23.2\designer
- Container command: Launching the container with: docker run -it -v ${PWD}:"C:\builds" afl-touchgfx:2.0 powershell.exe
- Command approaches:
-> powershell -Command 'C:\TouchGFX\4.23.2\designer\tgfx.exe generate -p C:\builds\TouchGFX'
-> powershell -Command 'C:\TouchGFX\4.23.2\designer\tgfx.exe generate -p C:\builds\TouchGFX'powershell -Command 'C:\TouchGFX\4.23.2\designer\tgfx.exe generate -p C:\builds\TouchGFX'
Throws the error: Object reference not set to an instance of an object.
Notes:
I have checked a similar issue as someone reports changing locale but both locales are set the same (checked with Get-WinSystemLocale, both are en-US English (United States))
Have tested both with .touchgfx file UTF-8-BOM and UTF-8
Thanks in advance for your help