2024-09-20 5:17 PM
Hello,
i am working on a board that is redrawn from the H745I-Disco which originally has the FT5336 as touch controller. My Display has the FT5426. On an earlier board that recreated the F746-Disco (which also has the FT5336) i noticed that the FT5426 worked right away. This was not the case on the H745 but was fixed after changing the Device ID. So touches are detected and deliver the proper values for x and y in sampleTouch() but nothing reacts to it. It is like there is no touch functionality at all. Any recommendations?
Thanks in advance!
Martin
Solved! Go to Solution.
2024-09-29 1:36 AM
Hi Gaetan,
thank you very much for your reply. You summarized my problem correctly. The thing that didnt catch my eye right away was that x and y coordinates where swapped. As soon as i assigned x to y and y to x it started working.
The difference between the FT53 and FT54 seems to be quite a bit more but since there is no multi touch in touch gfx it can be a cheap workaround i guess and it works from a user perspective.
Thanks for your effort!!
2024-09-27 5:40 AM
Hello @MReus.2 ,
To summarize:
Are you sure that your GUI has clickable area?
Are you sure that your screen has touch?
Do you hand touch coordinates to the touchgfx framework,
Can you share your sampleTouch() function?
Regards,
2024-09-29 1:36 AM
Hi Gaetan,
thank you very much for your reply. You summarized my problem correctly. The thing that didnt catch my eye right away was that x and y coordinates where swapped. As soon as i assigned x to y and y to x it started working.
The difference between the FT53 and FT54 seems to be quite a bit more but since there is no multi touch in touch gfx it can be a cheap workaround i guess and it works from a user perspective.
Thanks for your effort!!
2024-09-30 2:09 AM
Hello @MReus.2 ,
I am glad you resolved your problem! :smiling_face_with_smiling_eyes:
Regards,