My update wishlist
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-20 6:12 PM
If you guys are working on a new version update anytime soon, here are some things I'd like to see.
- Add standard shortcut keys to the top menu (Alf-F, Alt-E, Alt-H)
- When creating a new application, use a standard File dialog for the Application Directory so you can paste/edit a path. And it should remember the last path!
- Shortcut keys for Run Simulator, Run Target, Generate code (F5, F6, F8)?
- Add an orientation setting at the application node (and most of the json project settings)
- Move the build output window into a docked view, instead of a popup.
- When opening a project from the recent list, use a loading progress rather than hardlocking the UI on the main thread for 30 seconds.
- Help => Link to help documents / knowledge base for Designer
- Help => Check for Updates
-or-
Open source the Designer to Github and let the community work on it.
Labels:
- Labels:
-
TouchGFX
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-22 12:00 AM
Hi @Community member,
Thanks for the suggestions! - I'll pass them along to the Designer team.
Some of these features you are requesting are already underway!
/Anders