2021-10-12 06:48 AM
We are planning a new project and would like to know if the following configuration would work:
Has anyone experience with HyperRAM and HyperFlash in multiplexed mode together with TouchGFX? Is that possible? If so, are there any pitfalls?
Any comments are very much appreciated!
Best regards
GS
2023-02-10 10:52 AM
I am considering pretty much the same setup.
Did you get it up and running?
2023-02-12 05:33 AM
Hi Southbranch,
to be honest, we had a certain delay in this project. But it will be ramped up within the next months. I hope to get it up and running then - fingers crossed. The HyperRAM is working in another project - but this has no TouchGFX and no HyperFlash included. The key for the Flash will be to have the download programmer working for Keils ULINK Pro.
I will report as soon as I can tell more.
BR GS
2023-02-12 07:38 AM
or use tft with built in controller, as i do;
i have here 7" TFT, 800x480 pix, touch , with EVE controller and SPI connected to stm32H7A3 board;
read about displays with such controller, so you can play even video ;
displays with EVE :
https://riverdi.com/product-category/intelligent-displays/bt817q/?pr=22829
https://www.matrixorbital.com/eve3-70a
and the library i use is by Rudolph :
https://github.com/RudolphRiedel
https://www.mikrocontroller.net/topic/395608
2023-02-12 07:49 AM
We already have selected the LCD (and already have the panels in stock) and we are definitely using TouchGFX, which is a great tool to design our screen menus and to operate through our complex user interface.
Our main question is about the configuration with HyperFlash and HyperRAM.