2022-12-29 7:46 AM
How can I use multiple events or multiple mixins in touchgfx. I've managed to use only one so far (like here). If I want to use several, I can't pass 2 callbacks to the view's constructor (in Screen1View.cpp).
Screen1View::Screen1View():boxMoveAnimationEndedCallback(this, &Screen1View::boxMoveAnimationEndedHandler), boxClickedCallback(this, &Screen1View::boxClickHandler) { }When i select an event in touchgfx the following structure can be see
(in Screen1ViewBase.hpp).
touchgfx::MoveAnimator< touchgfx::Box > box1;If I use several, the structure is different
touchgfx::ClickListener< touchgfx::MoveAnimator< touchgfx::Box > > box1;Does somebody has any idea? is it even possible to use multiple mixins?
2023-01-02 1:57 AM
Hello RReit.1,
Yes it's possible to use multiple mixins. Let's say you have a TextureMapper (that we call myTextureMapper) with both ClickListener and MoveAnimaor mixins.
In your hpp file file you need to have something like this:
//Declaration of needed Handlers
virtual void textureMapperAnimationEndedHandler(const AnimationTextureMapper& src);
virtual void textureMapperClickHandler(const touchgfx::MoveAnimator< touchgfx::AnimationTextureMapper >& b, const ClickEvent& e);
//Callback for Texture mapper : triggered when animation ends
Callback<FactoryView, const AnimationTextureMapper&> textureMapperAnimationEndedCallback;
//Callback for Texture mapper : triggered when clicked
Callback<FactoryView, const touchgfx::MoveAnimator< touchgfx::AnimationTextureMapper > &, const ClickEvent&> textureMapperClickedCallback;Then in your cpp , you'll pass it to the constructor like this :
Screen1View::Screen1View() :
textureMapperAnimationEndedCallback(this, &FactoryView::textureMapperAnimationEndedHandler),
textureMapperClickedCallback(this, &FactoryView::textureMapperClickHandler)
{ }And then you'll associate the widget to the callback in the setupScreen() function for example :
void Screen1View::setupScreen()
{
myTextureMapper.setTextureMapperAnimationEndedAction(textureMapperAnimationEndedCallback);
myTextureMapper.setClickAction(textureMapperClickedCallback);
}Hope that helps.
/Osman
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.