cancel
Showing results for 
Search instead for 
Did you mean: 

Simulator won't compile if BSP header files are included in user xxxxView.cpp file 4.21.0 TouchGfx 1.11.0 Cube IDE

WBreg.1
Associate II

Hi all,

just a very basic test application and a basic question:

Setup:

Design a GUI with a button creating a virtual function as inetraction

Open project in IDE, add virtual function to the xxxView.hpp and xxxView.cpp.

Include the appropriate board support package in order to toggle a LED.

Put the BSP_LED_Toggle() in the virtual function.

Initialize the BSP_LED in the main.c

Run it from IDE - works like a charm

Problem:

Once done this, the simulator won't compile any more giving this error message:

Quote:

fatal error: stm32469i_discovery.h: No such file or directory

End of Quote:

Question:

Is there an easy and consitent way to tell the simulator where to find the file (i.e. all include files present in the project, as for the IDE)

I suppose that the Project configuration in touchGFX might be the right place.

But i'm not all too familiar with the overall project setup concerning the simulator.

Can anybody help?

Best regards,

Wolf

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
WBreg.1
Associate II

Edit:

BTW, to make it easier to reproduce:

This also happens when you edit an interaction in a button object where you place an include directive in the "Includes" field. (i.e.: #include "stm32469i_discovery.h").

Here again, the project will compile and work OK for the target, but will not compile for the simulator. Error as in my previous post.

Best regards

Wolf

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.