cancel
Showing results for 
Search instead for 
Did you mean: 

Missing documents and Support for New MCUs in STM32F4 family -- STM32F429/F439

ee1
Associate II
Posted on July 24, 2013 at 07:54

From the ST website, I came to know about new additions to the STM32F4 family. These are

STM32F4

29

/4

39 series MCUs. Their data brief tells that they have LCD-TFT controller and Chrom-ART Accelerator. These are highly valuable features for my project which is in initial Design phase.

My problems are:

  1. The STM32F4 reference manual should now have details of the above mentioned peripherals, just like it details all other peripherals. Unfortunately, this doesn't seem to be the case.

  2. Is there any development board featuring one of these new exciting micros? Is any board coming soon? (Preferably a low cost one like Discovery boards)

  3. Leading suppliers like farnell and digikey don't have any parts of this series in their listing. 

    Are these parts selling in market? if no, when they are expected?

Any help regarding these problems will be appreciated.

Thanks in anticipation.

#stm32f429 #lcd-tft #discovery
10 REPLIES 10
a_rocchegiani
Associate II
Posted on September 20, 2013 at 20:46

Thank you Clive for the links,

I download the package, the library do not have its native help file but I already 'doxigenate' it for a  first analisys of the new modules.

Thank again.