2021-01-21 12:57 PM
Hello,
I want to download sample code from this page: https://support.touchgfx.com/docs/development/ui-development/touchgfx-engine-features/backend-communication
But I don't think the links are working, for example:
http://sw-center.st.com/touchgfx/TouchGFX/knowledgebase/hw_integration_tasks_exti.4.9.3.zip
Does not download the zip. I think the links maybe broken again.
Is there an updated link we can use to get the example code?
Thanks!
Solved! Go to Solution.
2021-01-22 05:41 AM
Hi Romain,
Thanks for the response and hint! I was able to download from another browser.
The browser I was using was Chrome version 87.0.4280.141 (Official Build) (x86_64).
When it was not working, none of the .zip download links on the page seems to work.
/RR
2021-01-22 12:51 AM
Hi,
This is very odd as I am able to download it on my side. What browser are you using ? Do the other links work or is it only that one in your case ?
/Romain
2021-01-22 05:41 AM
Hi Romain,
Thanks for the response and hint! I was able to download from another browser.
The browser I was using was Chrome version 87.0.4280.141 (Official Build) (x86_64).
When it was not working, none of the .zip download links on the page seems to work.
/RR
2021-01-25 06:42 AM
Good to hear that you were able to download the zip you needed. I'll try to see if I can replicate that issue with the same Chrome version when I can just to check 👌.
/Romain