2025-06-30 2:27 PM - last edited on 2025-07-09 3:49 AM by Andrew Neil
Hello!
I wanted to ask if theX-NUCLEO-GFX01M2 module is compatible with STM32 NUCLEO-H533RE? The official documentation does not say anything about this NUCLEO board.
Kind regards
Andrew
Solved! Go to Solution.
2025-07-03 1:18 AM
Hello @a_niedworok2 ,
Yes this X-NUCLEO-GFX01M2 shield is compatible with STM32 NUCLEO-H533RE.
2025-07-03 1:18 AM
Hello @a_niedworok2 ,
Yes this X-NUCLEO-GFX01M2 shield is compatible with STM32 NUCLEO-H533RE.
2025-07-05 9:27 AM
Thank you for the information.
Is there a driver available for this LCD for the H533?
Andrew
2025-07-09 3:46 AM
The display driver is the same as the other small NUCLEO TBSs (like the NUCLEO-G071RB TBS for instance).
However, if you intend to use the external flash (the one in the display shield), then you would need to create an external loader and use it when flashing your board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.