Skip to main content
Associate III
January 22, 2024
Solved

GPU2D not available when using L8 Pixel Format

  • January 22, 2024
  • 2 replies
  • 1057 views

Hi, I am using an STM32U5A9ZJT with LTDC L8 buffer and cannot select GPU2D, is support for L8 being added soon?
Being able to use L8 and vector fonts would be ideal for storage savings.

 

I also noticed that the "hardware" option for vector rendering is available on the STM32U5A9, isn't this a feature of the NeoChromVG of the STM32U5G9?

 

Can I use L8 images in touchgfx when using an RGB565 buffer? I tried this and it works in the emulator but crashes on device.

 

This topic has been closed for replies.
Best answer by LouisB

L8 format is not supported by GPU2D TouchGFX on NeoChrom/NeoChromVG | TouchGFX Documentation

2 replies

PhilipCAuthor
Associate III
January 24, 2024

also seen 4.23.1 is now out, i downloaded and installed it but in cubemx it still says 4.23.0

PhilipC_0-1706135088420.png

 

LouisBBest answer
ST Employee
July 9, 2025
Louis BOUDOST Software Engineer | TouchGFX