2019-02-21 4:52 AM
I am implementing a settings menu for my particular project I decided to use a common button for rising and descending the values of the parameters but I cant catch which page which is containing the parameter desiring to configure ,swiped
2019-02-22 5:05 AM
Hi @özcan sahsuvar,,
Have you checked the SwipeContainer example from within the designer? It supports a page indicator at the bottom of the screen to show which element is in focus.
Hope that helps,
Best regards,
Martin
2019-02-22 5:42 AM
void Screen3View::plusValue()
{
if(swipeContainer1.pageIndicator.currentPage == 0x00)
{VLabelling_Speed++;}
if(swipeContainer1.pageIndicator.currentPage == 0x01)
{VLabelOffset++;}
if(swipeContainer1.pageIndicator.currentPage == 0x02)
{VDelayAfterSee++;}
Unicode::snprintf(SpeedTextBuffer, 5, "%d", VLabelling_Speed);
SpeedText.invalidate();
Unicode::snprintf(OffsetTextBuffer, 5, "%d", VLabelOffset);
OffsetText.invalidate();
Unicode::snprintf(DelayTextBuffer, 5, "%d", VDelayAfterSee);
DelayText.invalidate();
}
thank you very much for your reply but I did something to get job done but I am not sure it obeyed the work flow. Page indicator class is a private object in the swipecontainer class I had to cut it from private area and paste under public: in the swipeContainer.hpp file in the code snap I am calling that function and it has to determine which page selected. If I did something wrong or something out of workflow please warn me.
2019-02-22 6:49 AM
Hi @özcan sahsuvar,
It's true that the indicator is private. I suppose one could want to get the current page or even receive an event/callback when a page has been changed. You haven't changed any behavior, so you could keep doing it like that - or create your own custom OzcanSwipeContainer that simply defines an additional uint8_t getSelectedPage(). It's up to you.
Best regards,
Martin
2019-02-24 10:01 AM
is there any example of custom swipecontainer I dont know where to start. Unfortunately pageIndicator.currentPage does not return me convenient value