cancel
Showing results for 
Search instead for 
Did you mean: 

Is the development environment of STM32H7 & TouchGFX similar to STM32F7?

YJMoon
Associate III

Hello.

I was developing a GUI with STM32F767 & RGB TFT LCD.

However, the specification has changed and I should consider changing to the STM32H743.

Are there any issues to watch out for when changing the cpu?

Does CubeIDE & TouchGFX Deginer support H7 development environment?

If yes, which version can I use?

Thanks for your help.

1 ACCEPTED SOLUTION

Accepted Solutions
Romain DIELEMAN
ST Employee

Hi,

TouchGFX does support H7 development. There is an application template within Designer for the H743 eval board, you can have a look at it and get some inspiration to set up your configuration.

Concerning potential issues when changing cpus, I don't know sorry :beaming_face_with_smiling_eyes:.

/Romain

View solution in original post

3 REPLIES 3
Romain DIELEMAN
ST Employee

Hi,

TouchGFX does support H7 development. There is an application template within Designer for the H743 eval board, you can have a look at it and get some inspiration to set up your configuration.

Concerning potential issues when changing cpus, I don't know sorry :beaming_face_with_smiling_eyes:.

/Romain

Thanks for your answer. It’s a good thing TouchGFX supports H7.

Have a nice day!

/YMoon

Thanks, you too ^^