cancel
Showing results for 
Search instead for 
Did you mean: 

is possible to use one modal window for multiple screens?

tliao.1
Associate II

the modal window is likes message box that I needed.

I have multiple screens in project, can I use a same modal window for all screens or I need to add a modal window into the every screen?

how to do that if all screens can share a same modal window?

is someone can tell me? thanks.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
HP
Senior III

The short answer is no - you cannot reuse the same modal window.

I think the easiest approach here would be to design a container with everything you need and then add that to the modal you want to show.

the long answer is that there is a way to re-use containers (or other widgets for that matter) but it's not straight forward.

Hello tliao.1,

As HP mentioned, using custom containers are a possibility. Simply creating a modal window inside a custom container and adding the custom container to each screen. But in the end it will still be different instances of the "same" modal window since every widget in a screen are only alive/allocated when this screen is displayed. When changing screen the widgets are destroyed.

/Alexandre