2024-08-10 07:30 AM
The SVGImage widget is a great tool but, as I understand it can only use SVG images from the SVGdatabase.
I may imagine to subclass the SVGImage class and handle directly run time created lists of VGObject as it is done with the SVGdatabase.
What is missing is to have the imageconverter tool code to run on the embedded platform. I mean the code that convert XML SVG text files to the VGShape , commands and points like those found in SVGDatabase.cpp.
Could this code part be disclosed or a new function like 'dynamicSVGCreate( )' be added to the lib.
This function could return a VGObject being given a text string with the SVG content ?
Or do someone have an other solution to dynamically decode SVG XML text to bitmap ?
BR
Pierre