2019-10-01 1:27 AM
Hi.
The problem is
The project is in the memory of mcu (flash).
button - OK
The project is in the memory of QUADSPI.
what could be the problem?
Добрый день.
Проблема �?ледующа�?...
Е�?ли пиши проект в mcu, отображает�?�? корректно. Е�?ли на флешку, то пропадает цвет кнопок.
Что может быть не так �? проектом???
Видео и проект во вложение.
2019-10-02 11:13 AM
All PNG files from the toucgfx demo project
2019-10-02 4:58 PM
Hello,
I see you are using a custom hardware (QSPI W25Q128 and others). Did you run sort of validation tests to make sure writing and reading from the QSPI is fine?
With regards,
Badreddine
2019-10-03 3:16 AM
2019-10-03 3:22 AM
These files are displayed correctly.
These files are not displayed correctly.
(png with transparent background)