2025-01-05 12:19 PM
Hello,
I'm currently working on a project where I want to use both the NFC08A1 expansion kit and the RVA35HI display kit along with the U575ZI-Q development board. When I try to include the X-CUBE-TOUCHGFX software package in STM32CubeIDE, I get the following message in the software packs component selector
I understand that there are pin conflicts between the two software packs. I have tried reassigning all the pins of the X-CUBE-NFC6 such that there are no conflicts, however even after doing so I get the same warning
Any idea on how to go about from here?
Cheers