cancel
Showing results for 
Search instead for 
Did you mean: 

in TouchGFX how to change the default application directory to anything but "C" ?

David.Yves
Associate II
 
13 REPLIES 13

​Oh, you mean because you can't have spaces in the project folder?

​If you could provide some detail on your issue i'll use it as ammunition when i talk to the designer guys about it :)

Hi,

I posted the original request WBW(way back when) and I found the solution

I don’t use TouchGFX anymore

Ps you can remove me from the distribution list of touchgfx

@Martin KJELDSEN​ , correct. Spaces are disallowed in the TouchGFX project folder. Image attached to show the error.

@David.Yves​ use the thread controls to mute the conversation if you don't want updates.