‎2020-01-16 4:10 AM
Hi there
Today I wanted to try the L8 image format. After generating the assets I flashed the STM32H750-DK.
I have a startupscreen with a fade transistion. Now with the L8 image format the screen is stuttering a lot. I also have a scroll list, which is not usable because of the delay.
I this behaviour to be expected?
Is there anything to be done to use L8 image format?
One side note: I have deactivated caching until our development is finished. When D-Cache is activated, the performance is a lot better.
Thanks for your help @Martin KJELDSEN​ =)
‎2021-05-25 2:09 AM
Check out this article on L8:
Using the L8 Image Format to Reduce Memory Consumption | TouchGFX Documentation
‎2021-05-25 2:55 AM
This is just the explanation about L8 principle.
I need the L8 PNG file format.
‎2021-05-25 3:19 AM
Okay. Wasn't clear. Still not 100% clear, but here's some more info that will get me closer =)
Why do you need to know the format? Do you want to write your own image converter? We support four different 8-bit framebuffer formats . When using LTDC the CLUT for each format is programmed directly and is not a part of the image. This is handled by the generator.
ARGB2222
RGBA2222
BGRA2222
ABGR2222
/Martin
‎2021-05-25 3:36 AM
Yes,I want to write imageconverter.
Like the PNG image file,it has the standard format,like IHDR block,IDAT block and chunk and so on.I need these info.
I saw the chapter "Using L8 Images in TouchGFX Designer",the TouchGFX will generate a L8 format image,and is this image saved as a L8 image file?What is the file format?If it is not file,how does the L8 image been stored?
‎2021-05-25 6:13 AM
You can probably just inspect one of the generated pngs =) Just pick one of the L8_ image formats from the designer and look inside the TouchGFX/generated/assets/images/ folder. The color lookup table is provided on the side.