2021-08-20 06:27 AM
Hello,
I am trying to setup a IAR 8 project using TouchGFX Designer 4.17.0
When I open the generated project in IAR Workbench, it fails to build.
What I do:
Then I get a lot of compile errors
When I run the code on the board using "Run Target" in TouchGFX Designer, the code runs fine (and no build errors or warnings).
Versions:
Board: STM32H7B3I-EVAL
Are there issues with TouchGFX Designer 4.17.0, or am I doing something wrong?
Regards, Jan
2021-08-23 03:41 PM
Hello JRoyn.1,
Indeed you are missing one step 🙂
What you should do :
Hope this helps,
/Alexandre
2021-08-24 12:04 AM
Hello,
Thanks, that helped. Code builds and run on the target now.
However, still some warnings:
When I open the project in STM32Cube the first time:
Need to upgrade from 1.9.0 to 1.9.0?
Choosing "Continue" worked fine.
When downloading code to target using IAR Workbench:
Tue Aug 24, 2021 08:51:26: Flash download warning: 18972 out of 18972 bytes from data record CODE:[0x90000000,0x90004A1B] will not be flashed
Tue Aug 24, 2021 08:51:26: There were warnings while generating flash loader input.
Tue Aug 24, 2021 08:51:26: See the Debug Log window for details.
Tue Aug 24, 2021 08:51:28: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 8.4_2\arm\config\flashloader\ST\FlashSTM32H7xx.mac
...
Tue Aug 24, 2021 08:51:34: Warning: Verify error, failed to read memory at address 0x90000000 - 0x90003FFF
Tue Aug 24, 2021 08:51:34: Warning:
Tue Aug 24, 2021 08:51:34: Verify error at address 0x90000000, target byte: 0x11, byte in file: 0x00
Tue Aug 24, 2021 08:51:34: Warning:
Tue Aug 24, 2021 08:51:34: Verify error at address 0x90000004, target byte: 0x18, byte in file: 0x00
...
Tue Aug 24, 2021 08:51:36: Hardware reset with strategy 0 was performed
Tue Aug 24, 2021 08:51:36: Target reset
Tue Aug 24, 2021 08:51:36: There were 1 error and 2 warnings during the initialization of the debugging session.
The warnings does not seem to create any issues though.
Thanks for help,
Regards, Jan
2021-08-25 07:52 PM
Hello JRoyn.1,
Data record code not being flashed might not be a big issue for your application to work, although not really sure on that point.
Maybe you can try with CubeMX 6.2.1 instead and see if it produces the same issue.
/Alexandre
2021-09-09 02:11 AM
Hi,
When working with IAR or Keil you should not use the "Run on target" option from those tools otherwise you will not use the external flash loader for your ST board as shown in the warning message. You should use STM32CubeProgrammer instead: make sure to go to the External Loader section and select the right one for your board. In your case it should be the MX25LM51245G_STM32H7B3_DISCO.stdlr .
/Romain
2021-09-09 02:14 AM
It should be the MX25LM51245G_STM32H7B3-EVAL-REV<A or B depending on your board revision>.stdlr in your case sorry, not the one for the discovery kit.
/Romain