cancel
Showing results for 
Search instead for 
Did you mean: 

I'm implementing TouchGFX on a Custom BoardI detected that the RAM DQS Pin(OCSPI2_DQS) is always low and does not work.

MLuis.1
Associate III

I'm implementing TouchGFX on a Custom Board using the same circuit as the STM32H735G-DK for the external memories. I detected that the RAM DQS Pin(OCSPI2_DQS) is always low and does not work. The display is always grey as the framebuffer is not written properly.

The display is working well, I tested it by using an internal framebuffer.

My project is attached.

2 REPLIES 2
Not applicable

Post link deleted to adhere community guidelines.

MLuis.1
Associate III

The hardware is all correct in terms of the circuit. I checked all the lines with an appropriate oscilloscope and all are working fine except for the DQS on the RAM. All the memory components are the same as the STM32H735G-DK board as well as the firmware configuration.