cancel
Showing results for 
Search instead for 
Did you mean: 

I can't generate code with touchGFX due to .cproject file.

massimoperdigo
Associate III

 

Hi everyone,

I’m experiencing some frustrating issues while trying to generate code for a blank project using TouchGFX with the STM32H757XIHX dual-core.

When I attempt to generate the code, I receive an error indicating that it cannot locate the .cproject file. I’ve generated this project using the IDE, which I really hate; Although TouchGFX supposedly supports Makefile as a toolchain, when I try to generate the code with Makefile, it throws an error stating that the toolchain is not accepted.

This leaves me with no option but to rely on the IDE, which generates a folder structure where the .cproject is located within the CM7 subproject. It seems that TouchGFX is looking for the .cproject in the root directory, where it’s not present.

Can anyone guide me on how to change the path or resolve this issue? I would really appreciate any help!

Although, if someone knows how to use TOUCHGFX with the Makefile as a toolchain (selected option in cubeMX instead of IDE), please let me know!! I do not want to use this useful tool.


root:

massimoperdigo_0-1730118651105.png

CM7

massimoperdigo_1-1730118675053.png

thanks

 

1 ACCEPTED SOLUTION

Accepted Solutions

Great, I am glad it worked! :smiling_face_with_smiling_eyes:

 

I took a TBS we made, opened STM32CubeMX, selected Makefile toolchain, generated code in STM32CubeMX.
Then I opened TouchGFX Designer, added a screen and clicked on the generate code button.
I got an error message but it is in the "Post Generate Target" and the "Generate code", "Generate Assets" and "Post Generate" worked fine.
There is only an issue in the "Post Generate Target" which takes core of the files for the target, so the files for the compilation, etc (gcc, IAR, Keil, etc).
I checked the folder and I was able to see the new screen that I have added.
So even though I get an error message, everything I need is still there and it probably is the same for you.

Now you have to compile and flash using your custom Makefile.

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

View solution in original post

8 REPLIES 8
GaetanGodart
ST Employee

Hello @massimoperdigo ,

 

So now, instead of selecting Makefile for the toolchain, you select STM32CubeIDE before generating code?

What makes you think that TouchGFX is looking for the .cproject in the root?
In our TBS, in the root, we have a folder called STM32CubeIDE where whe have the .project and the .cproject.
But for you, you have the .project in double.
Can you try to move the .cproject to the root manually (and maybe delete the .project in that is in the CM7 folder)?

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)
massimoperdigo
Associate III

I will try it. However, it is possible to create a project with cubeMX and generate code using Makefile toolchain? and then, make use of touchGFX designer to develop my GUI?

Hello @massimoperdigo ,

 

Yes you can use the Makefile toolchain, then create a GUI using TouchGFX Designer, then click on "Generate code" from TouchGFX Designer and then compile and flash using your own files.

Did changing the location of the file have any impact?

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

Yes, I changed the location manually and the first problem disappeared (cannot locate the .cproject file). however,

now, when I generate code from touchGFX, it shouts an error saying that Makefile toolchain is not supported...

Great, I am glad it worked! :smiling_face_with_smiling_eyes:

 

I took a TBS we made, opened STM32CubeMX, selected Makefile toolchain, generated code in STM32CubeMX.
Then I opened TouchGFX Designer, added a screen and clicked on the generate code button.
I got an error message but it is in the "Post Generate Target" and the "Generate code", "Generate Assets" and "Post Generate" worked fine.
There is only an issue in the "Post Generate Target" which takes core of the files for the target, so the files for the compilation, etc (gcc, IAR, Keil, etc).
I checked the folder and I was able to see the new screen that I have added.
So even though I get an error message, everything I need is still there and it probably is the same for you.

Now you have to compile and flash using your custom Makefile.

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

Hello @massimoperdigo ,

 

Have you been able to move forward on your issue?

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)
alirezaSalehi
Associate II

hello, I have the same problem.

as you mentioned earlier, I copied .cproject to the main project folder, and touchgfx generated code without a problem.

but when I build project in the cubemxIDE, I get several Errors that are related to directories I think. ((fatal error: touchgfx/Bitmap.hpp: No such file or directory) and other directories))

I think this way is wrong for solving this problem. (copy .cmake file in other directories.)

could you explain me how to solve this problem? I would appreciate any help!

alirezaSalehi
Associate II

Hello everyone!

For TouchGFX in dual-core, we have to create a project in STM32CubeMX and generate it in unchecked "Generate under root."

thanks.