cancel
Showing results for 
Search instead for 
Did you mean: 

I am working on a project related to printer design. however, I can't figure out certain functions can run on touch gfx or not. I have explained in detail the desired work. So that I could know whether ican implement this project through touch gfx or not.

SAMIN.1
Associate III

I have attached a sample video, in which my desired work is being implemented.

implemented in the sample video.

As you can see the user can increase or decrease the text and can change the height and width at runtime as he wants.

Can we implement similar things in touch gfx ?

secondly, the user can add multiple texts in the box wherever he wants and return every parameter of the box x, y-axis, height, and width.

thirdly the box size is automatically resized according to the number of digits in it.

Kindly guide us, is nextion intelligent series is capable of doing these tasks?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MM..1
Chief III

Can we implement similar things in touch gfx ?

Maybe yes , but basic reply is TGFX dont have support for dynamic font size , then no.