cancel
Showing results for 
Search instead for 
Did you mean: 

I am trying to use an external source and header file IconFlags.c and .h but cant call the header file IconFlags.h from any program but can call functions in IconFlags.c without including the header file. But in Model, View etc the funct are not called.

Amaresh
Associate III

0693W00000KaLKxQAN.jpg

1 REPLY 1
Amaresh
Associate III

Im using the current version of touchgfx and open the IDE after making a touchgfx project. I cant drag the header file into the includes also. How do I include the .h file into the project so I can use the functions of IconFlags.c in Model, View etc?

ps.-

When I try to include the header file alone or with the path it says it doesn't exist but can call the functions from the main when it is not included which is weird.